AXIS#.VL.AINDEC

Description

Defines the deceleration ramp when the axis is in Analog Command Source, and Velocity Mode.


  • This keyword has no effect when the drive is in Torque or Position mode.

Versions

Action Version Notes
Implemented 02-01-02-000

General Information

Type

Read/Write

Description Describes the acceleration ramp for the velocity loop.
Units

Rotary: RPM/s, RPS/s, deg/s2, (custom units)/s2, rad/s2

Linear: counts/s2, mm/s2, µm/s2, (custom units)/s2

See Acceleration Units for details.

Range

Depends on units. See Acceleration Units for details.

Default Value

10,000 RPM/s

Depends on units. See Acceleration Units for details.

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

CAN bus drives: AKD2G-SPC

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.VL.AINDEC

5011h

22h

Unsigned32

Acceleration 16Khz

-

Read/Write

No

AXIS2.VL.AINDEC

5111h

22h

Unsigned32

Acceleration 16Khz

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.VL.AINDEC

6039

1797

Signed32

Read/Write

Acceleration

AXIS2.VL.AINDEC

71575

1179

Signed32

Read/Write

Acceleration

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.AINDEC

6039

Float

Read/Write

Acceleration